EDMUND WEBINAR SERIES
See All WebinarsJoin us for a 30-minute webinar presented by Edmund Optics' experts Kasia Sieluzycka and Dr. Pierre-Alain van Griethuysen to learn about the different considerations needed for designing custom aspheres.
Request Content
Aspheres used for light collection, light focusing, and reducing the number of elements in a system can take different forms and each application requires a very specific set of design considerations and specifications.
At the conclusion of the webinar, participants will have a strong understanding of:
Kasia Sieluzycka
Senior Solutions Engineer
Kasia is a Sr. Solutions Engineer at Edmund Optics in Tucson, AZ, USA. She has over 10 years of experience working directly with customers to specify cost-effective optical solutions for a variety of applications from the life sciences to aerospace, with a focus on custom optical components. She holds a B.S. and M.S. in Optical Engineering from the University of Arizona.
Dr. Pierre-Alain van Griethuysen
Product Line Manager, Precision Optics
Pierre is a Product Line Engineer at Edmund Optics in York, UK. He joined Edmund Optics in 2020 and has worked in the Strategic Optical Innovations Businiess Line, developing standard products and assisting with expansion of custom capabilities. Pierre has a background in bioscience and received a PhD in Biology from the University of York.
ou consulter les numéros d’autres pays
facile à utiliser
entrer les numéros de stock pour commencer
Copyright 2023 | Edmund Optics, Ltd Unit 1, Opus Avenue, Nether Poppleton, York, YO26 6BL, UK
POLITIQUE DE CONFIDENTIALITÉ | POLITIQUE DE COOKIES | CONDITIONS GÉNÈRALES | CONDITIONS GÉNÈRALES B2C | MENTIONS LÉGALES | ACCESSIBILITÉ
L'entreprise Edmund Optics GmbH en Allemagne agit comme un mandataire d'Edmund Optics BV aux Pays-Bas.
Le titulaire du contrat est Edmund Optics BV aux Pays-Bas.
Ce contenu peut comporter des éléments générés ou modifiés à l'aide de l'intelligence artificielle (IA).
The FUTURE Depends On Optics®