Beam expanders, whether Galilean or Keplerian style, can be used in reverse. There are however several factors to consider before doing so. The first factor is alignment. The exiting aperture will now be much smaller than the entrance aperture, making any tilt in the alignment pronounced. The second factor is clipping. All laser beam expanders will have a limit to the acceptance angle of the smaller optic. For example, in the case of our Fixed Power HeNe Beam Expanders, the largest beam that can exit the system is 27mm. Thus when used in reverse, the largest beam diameter that can be accepted is 27mm. This condition applies to any expander system and should be supplied by the expander manufacturer. The third factor to consider is angle divergence. Although the beam is reduced by a magnification such as 10X, the divergence of the initial beam will increase by the same magnitude. Thus a 5mm diameter beam with 1mrad divergence will become a 0.5mm diameter beam with a 10mrad divergence. In cases where a laser or other light source must be kept as collimated as possible, the increase in divergence may be unacceptable. Fourth factor to consider is the increase in power density. Unless the optics in the laser beam expander are damage threshold tested, there is no guarantee that damage will not occur when reducing a mid or high power beam. If the laser beam expander is designed for high power density lasers, the damage threshold specification will be listed. For more information, please visit Beam Expanders.
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
This content may include material that has been generated or modified using artificial intelligence (AI).
The FUTURE Depends On Optics®