Glossary: K
Kellner Eyepiece
A type of eyepiece design consisting of a plano-convex field lens and a cemented doublet lens as the eye lens.
See also
Huygenian Eyepiece
, Periplan Eyepiece
, Wide-Field Eyepiece
Kerr Cell
Electro-optical device constructed from a crystal with attached electrodes used to modulate a laser beam. A phase delay of a laser transmitting through the crystal is modulated by applying a variable electric voltage, causing birefringence. The change is proportional to the square of the field, which is known as the Kerr effect.
See also Pockels Cell, Q-Switching
See also
Huygenian Eyepiece
, Periplan Eyepiece
, Wide-Field Eyepiece
Kinematic Mount
A type of optical mount capable of six degrees of freedom that are singularly constrained during alignment. It is designed to minimize stress to the optics or optical assemblies it holds.
Knoop Hardness
A measure of material hardness. A higher Knoop hardness corresponds to a stronger material.
ou consulter les numéros d’autres pays
facile à utiliser
entrer les numéros de stock pour commencer
Copyright 2021 | Edmund Optics SARL, 76-78 rue d’Alsace, 69100 Villeurbanne, France
L'entreprise Edmund Optics GmbH en Allemagne agit comme un mandataire d'Edmund Optics Ltd au Royaume-Uni. Le titulaire du contrat est Edmund Optics Ltd au Royaume-Uni.