Ultrafast Laser Applications: Short Pulse Revolution
Join representatives from Edmund Optics, TOPTICA Photonics, and Rochester Institute of Technology for a virtual discussion about the key benefits of ultrafast lasers and how they are revolutionizing fields as diverse as brain imaging and glass polishing.
Ultrafast highly-dispersive mirrors are critical for pulse compression and dispersion compensation in ultrafast laser applications, improving system performance.
The short pulse durations of ultrafast lasers lead to broad wavelength bandwidths, making ultrafast systems especially susceptible to dispersion and pulse broadening.
Understanding the most common laser sources, modes of operation, and gain media provides the context for selecting the proper laser for your specific application.
Laser induced damage threshold (LIDT) of optics is a statistical value influenced by defect density, the testing method, and fluctuations in the laser.
L’importance du diamètre du faisceau pour le seuil de dommage laser
Le diamètre d'un laser affecte fortement le seuil de dommage induits par le laser (LIDT) d'un composant optique, car le diamètre du faisceau influence directement la probabilité qu’un endommagement induit par le laser se produise.
Dispersion is the dependence of the phase velocity or phase delay of light on another parameter, such as wavelength, propagation mode, or polarization.
Dommages volumiques causés par le laser dans le verre
Learn why the bulk laser-induced damage threshold (LIDT) of glass is significantly different than the LIDT optical components with coatings, such as AR thin films.
Testing laser induced damage threshold (LIDT) is not standardized, so understanding how your optics were tested is critical for predicting performance.
Please select your shipping country to view the most accurate inventory information, and to determine the correct Edmund Optics sales office for your order.
ou consulter les numéros d’autres pays
facile à utiliser
entrer les numéros de stock pour commencer
Copyright 2023 | Edmund Optics, Ltd Unit 1, Opus Avenue, Nether Poppleton, York, YO26 6BL, UK
L'entreprise Edmund Optics GmbH en Allemagne agit comme un mandataire d'Edmund Optics Ltd au Royaume-Uni. Le titulaire du contrat est Edmund Optics Ltd au Royaume-Uni.